RTXC Application Notes on the Evaluator-7T Board
There are 2 projects for building the Example Applications for the Evaluator-7t: Eval7t_Dm and Eval7t_Ss. These will build a dual-mode and single-stack example, respectively. The dual-mode example exercises the multi-stack and single-stack features. There are nodes for building in Thumb or ARM modes. The Evaluator-7t examples were qualified with the Multi_ICE unit, with the MacGraigor Raven, and with the IAR J-Link USB.

Single-Stack Example

The single-stack example has 6 threads. One is a master thread. The other thread numbers 2 through 6 each cause a digit to be displayed on the 7-segment display of the Evaluator-7t board. For example, when thread 5 is fired off, the digit '5' is shown on the 7-segment display.